Downlink FRC Configuration
Bandwidth
Choices:
Downlink: Based on the Table 5.3.2-1 and 5.3.2-2 in 38.104
Uplink: Based on the Table 5.3.2-1 in 38.101-1 and 38.101-2
Selects the bandwidth configuration for the carrier.
Numerology
Selects the numerology of the configuration. The choices are related to the selected bandwidth.
Duplex Type
Choices: TDD | FDD
Selects the duplex type.
When TDD is selected, several TDD parameters appear below. These TDD parameters are reset to default values whenever numerology changes or FR changes. (The default values are different for each numerology.)
Transmission Periodicity
Sets the periodicity of DL-UL pattern. The choices are related to numerology.
Read-only.
Number of Downlink Slots
Sets the number of consecutive full DL slots at the beginning of each DL-UL pattern. The range is related to the numerology and slot configuration period.
Read-only.
Number of Downlink Symbols
Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP
Sets the number of consecutive DL symbols in the beginning of the slot following the last full DL slot.
Read-only.
Number of Uplink Slots
Sets the number of consecutive full UL slots at the end of each DL-UL pattern. The range is related to the numerology and slot configuration period.
Read-only.
Number of Uplink Symbols
Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP
Sets the number of consecutive UL symbols in the end of the slot preceding the first full UL slot.
Read-only.
Number of Special Slots
Displays the number of special slots.
Read-only.
TDD Slot Allocation
Displays the TDD slot allocation for one period.
Read-only.
FRC Type
Choices: QPSK | 64QAM | 256QAM
Default: QPSK
Selects the downlink FRC type.
OFDMA Channel Noise Generator
Choices: On | Off
Default: Off
Enable or disable OFDMA channel noise generator when setting downlink FRC.
Phase Compensation
For waveform playback mode:
Choices: Auto | Auto (Real-time) | Manual | Manual (Real-time) | Off
For real-time uplink mode:
Choices: Auto | Manual | Off
Default: Auto
Sets the phase compensation mode on baseband signal before upconversion.
Auto | Auto (Real-time): Use the RF frequency from the instrument node.
Manual | Manual (Real-time): Enter the RF frequency manually.
Off: Disable phase compensation on baseband signal.
(Real-time) means the phase compensation is done using FPGA inside the instrument.